Creating an automation
- On the Home page, tap
.
- Go to Automation and then tap
to create an automation.
- Tap
and choose an icon that best represents your automation.
- Enter a name of the automation (A) and select any of the
following conditions to meet (B).
- All conditions: All conditions must be met to trigger an automation
- Any condition: Any one of the condition must be met to trigger an automation.
- Tap Add conditions (C) and select
any of the following (D):
- Device status change (Select the device)
- Away Mode (Enable or Disable)
- Select Enabled mode away (E).
- To add an action, tap Then > Add an action and select any of the following. In this
case, Control a device (F).NOTE: Maximum 10 actions can be added.
-
Control a device: Select a device that you want to trigger.
-
Send notification: Turn on the notification for the automation.
-
Activate a moment: Select the moment that you want to trigger.
-
Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
-
- Select Schneider Charge (G) and then select an action (H) to assign.
- Tap Save (I).
The saved Automation is displayed on the Automation page. Tap the toggle switch on the Automation page to enable/disable the Automation.