DUG_Schneider Charge_WHP-01

Resetting the PIN via eSetup app

If the commissioning PIN code is lost, you can reset the PIN code to default value using the eSetup app.
  1. Open eSetup app and select Schneider Charge and tap Skip the tutorial.
  2. Power On the Schneider Charge, when the side LED indicator turns solid green tap Yes, it is green in the app.
  3. In Schneider Charge, when the side LED indicator turns solid green, press and hold the side push button for 3 s.
    This will create a temporary wireless network of the Schneider Charge which will be active for 4 min.
    NOTE: If the side LED indicator light is OFF, power OFF the charging station and then turn it ON to re-activate the side button.
  4. In the app, tap Yes, it’s breathing green and perform one of the following method to scan the QR code located on the side of your Schneider Charge to connect to the temporary wireless network.
    Open camera:
    Tap Open camera, on the pop-up message tap OK and scan the QR Code located on the side of charger to join the temporary wireless network.
    IMPORTANT: Make sure the camera permission is enabled for eSetup app.
    Connect manually:
    1. Tap Connect manually > Open Wi-Fi Settings.
    2. Select the SchneiderCharge_##-##-## from the list and enter Wi-Fi® password located on the side of the device.
    3. Once connected, return to the Wiser Home app.
  5. On the screen enter the New PIN, confirm the PIN and tap Save.
    NOTE: The PIN must contain 6 to 16 digits, cannot contain the same digit more than 3 times and code that should not have 6 sequential digits.
    New PIN is set successful.
  6. Enter New PIN and tap Reset PIN.
After reset, app displays the status.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?