DUG_Schneider Charge_WHP-01

Using the device

The Schneider Charge Panel allows you to start and stop charging and monitor the power consumption.

On the Home page, tap All > Schneider Charge to access the control panel.

On the Schneider Charge panel page, you can see the following:

  • Total cost of charging session (A).

  • Total time of charging in the session (B).

  • Total energy consumption in the session (C).

  • Control button (Start charging/Stop charging, Pause/Resume) (D).

  • Charging Mode (E).

  • Device settings (F) - You can rename the device or remove the device from the Wiser system. Refer to Renaming the device and Removing the device.

  • History (G).

Similarly you can control and check the current status of Schneider Charge from Home page.

  • Control button (H).

  • Current state of the device (I).

NOTE: Electric vehicles (EV) can't be charged immediately after they have stopped. Reconnect the plug to start charging. Refer Connecting/disconnecting the charger.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?