DUG_Schneider Charge_WHP-01

Away Mode

The Away Mode is designed to set your home in a state that is sensible when you are away for longer periods of time (e.g. being away for the weekend). It temporarily overrides the normal control (e.g. moments, automation) implemented in the Hub. When you disable the away mode, the controls revert to the state they where prior to entering the Away mode.

Set the Device State in Away Mode:

  1. On the home page, tap > Away Mode.

  2. Tap the toggle switch to enable/disable the device when in away mode.

    NOTE: The Heating setpoint feature is not available at this time.

Enable/Disable Away Mode

  1. On the home page, tap Automation (A).

  2. Tap Away Mode (B) to activate or deactivate the away mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?