Configuring - flat rate
- After reading the Tariff onboarding information. On the Tariff screen, tap Electricity.NOTE: If you have already configured your tariff settings, follow below menu navigation if you need to modify tariff rate.
On the Home page, tap . - Tap
(A) and select Flat.
IMPORTANT:-
Contract limit/Main incomer size is already set when pairing the main PowerTag as Grid. Refer to Pairing the main device.
-
If you like to change the contract limit/main incomer size, proceed to step 3.
-
- Tap
(B) to set the Contract limit/Main incomer size.
The Contract Limit/Main Incomer Size page appears.- Select your contract limit/main incomer size (kVA/A/kW)
from the drop down menu, then tap
and enter a value using the dial pad as per your country.
TIP: Default value is 63 A with range of 15 A to 160 A.A notification window will be prompted that the Contract Limit/Main Incomer Size is used by Anti-Tripping Management algorithm. If set incorrectly it may not work as expected and could result in the power tripping.
- Tap Continue, if you like to proceed.
- Select your contract limit/main incomer size (kVA/A/kW)
from the drop down menu, then tap
- Tap
(C) and select a subscription type (D) (refers to recurrent fee).
- Enter a value in the Cost ($) (E) field and tap Set.
- Tap
(F), enter a flat rate of consumption in the Rate - $/kWh field and tap Update.
- Tap Save (G).