DUG_Schneider Charge_WHP-01

Using Reduce My Bill

Using the Wiser Home app, you can view how the devices are controlled and scheduled for usage.

Control screen

On the Control Panel page, (A) denotes the next schedule for the device to switch on.

Schedule

when you select Reduce My Bill (A), In the next reduced bill period which is listed (B), the device will operate.

Away Mode

If you wish to activate Away Mode with Reduce My Bill. Away Mode will override Reduce My Bill commands based on high priority. For more information on Away Mode, refer to Away Mode.

Insights

To view how much money is saved through Reduce my Bill, refer to Insights.
NOTE: Savings will be shown as per what offer you have opted.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?