DUG_Schneider Charge_WHP-01

LED indication

Front Indicator Light

Charging station status

Solid White

Restart of the charging station – Please wait!

Breathing Green

Wi-Fi access point activated for commissioning

Blinking Green

Firmware upgrade on going – Please wait!

Solid Green

Ready

Breathing Blue

Charging on going

Blinking Blue

Charge suspension by the smart charging application or lack of remaining power in the house

Solid Blue

Charge suspension by electric vehicle or battery full

Breathing Orange

Not connected to the smart charging application when connectivity configured

Solid Orange

Locked

Solid Red

Stop/Error – Refer to trouble shooting section


Side indicator light

Charging station status

No light

PUSH button not activated - Power off and then back on the charging station to activate it

Solid Green

Ready to activate Wi-Fi access point for commissioning /

Blinking Green

Wi-Fi® access point activated for commissioning

Blinking Blue

Pairing mode with anti-tripping module (peak controller) activated

Blinking Red

Anti-tripping module power line communication or TIC communication (France only) lost

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?