Configuring - (peak/off-peak) rate
- After reading the Tariff onboarding information. On the Tariff screen, tap Electricity.
- Tap
(A) and select Time of use (peak /off-peak hours).
IMPORTANT: Contract limit/Main incomer size is already set when pairing the main PowerTag as Grid. Refer to Pairing the main device. If you like to change the contract limit/main incomer size, proceed to step 3. - Tap
(B) to set the contract limit/main incomer size.
- Select your contract limit/main incomer size (kVA/A/kW)
from the dropdown menu, then tap
and enter a value using the dial pad as per your country.
A notification window will be prompted that the Contract Limit/Main Incomer Size is used by Anti-Tripping Management algorithm. If set incorrectly it may not work as expected and could result in the power tripping.
- Tap Continue, if you like to proceed.
- Select your contract limit/main incomer size (kVA/A/kW)
from the dropdown menu, then tap
- Tap
(C) and select a Fixed charge type (refers to recurrent fee) -Yearly, Monthly, Weekly, Daily.
- Enter a fixed charge value in the Cost ($) field and tap Set.NOTE: The Fixed Charge is applied to recover the basic cost of electric service, independent of how much energy is used. These charges are electricity costs that don't change no matter how much electricity you use. This amount is fixed in your electricity bills.
- Tap
(D), enter peak rate of consumption in the Rate - $/kWh field and tap Update.
- Tap Add a rate.
- Enter the name of the rate in the text field (E).
- Enter a target value in the Rate - $/kWh field (F) and tap Add (G).
- Tap Add a Schedule (H) to set the time frame.
- Enter a schedule name in the NAME field. Example, Weekend tariff.
- Select the days of the week in DAYS field to apply the schedule.
- Tap
to set Start time and Finish time.
- Tap
and select a RATE TYPE.
IMPORTANT: It is necessary to set off-peak hours for each day per schedule (I) else you will not be able to save your tariff details. - Tap Add and then tap Save.