DUG_Schneider Charge_WHP-01

Managing the cable

  • Make sure that the charging connector and charging cable are securely stored between charging sessions.

  • Wrap the charging cable around the charging station’s cable trough.

  • If the Schneider Charge is installed outdoors, Remove the cap.

  • If the Schneider Charge is installed indoors, protect the connector by covering it with the dust cap.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?