DUG_Schneider Charge_WHP-01

Anti-Tripping Module

EVA2HPC1

EVA4HPC1

EVA2HPC3

Overview

Schneider Charge anti-tripping module, working in conjunction with a Schneider Charge charging station, forms an intelligent load management system that continuously adapts the charger's power output to the electric vehicle based on the available power in the home.

The power availability is calculated by the load management system by comparing the utility power limit and the home consumption gathered by a current transformer positioned on the bottom of the main circuit breaker.

The communication between the Home Anti-tripping system and the Schneider Charge charging station is done with power line communication, so no need to add a communication cable.

NOTE: Anti-tripping module is designed for use with the Schneider Charge. Do not use with other electrical devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?