DUG_Schneider Charge_WHP-01

Checking the device history

Using the Wiser Home app, you can monitor the cost and power consumption of the Schneider Charge by accessing the history.
To check the device history:
  1. On the Home page, tap All > Schneider Charge.
  2. On the device control panel page, tap History.
  3. In the History page, you can see the total power consumption per charging cycle and total charging cost.
    You can tap Load More to view the records of the past 30 days.
    IMPORTANT: If you have installed both PowerTag and Schneider Charge, you can monitor the powerflow and energy consumption in the Energy tab. For more information, refer to Live.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?