DUG_Schneider Charge_WHP-01

Connecting/disconnecting the charger

Connecting

  1. Plug in the charging cable connector into the EV Charger.

  2. Plug in the charging cable connector into the electric vehicle’s inlet.

  3. The EV Charger’s LED indicator will change from constant green to pulsing blue.

NOTE: For information on LED color, refer to LED indication.

Disconnecting

  1. Stop charging the vehicle with Wiser Home app to unlock the charging cable from vehicle socket.

  2. Unplug the EV Charger’s connector from the electric vehicle’s inlet.

  3. Wind the charging cable around the EV Charger winding trough.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?