Notifications and Alarms
Notifications and Alarms allows the Wiser Home app to send messages that show up in the notifications of your mobile device’s operating system and also you can set an alarm for overconsumption and no consumption of the specific device.
You can select the Notifications and Alarms in the Account options of the Settings menu.
-
Tap Notifications and Alarms (A).
Notification and Alarm settings:
| SYSTEM | |
|---|---|
| Low and Critical Battery |
Will notify you when the battery of a Device is low. |
| Offline Devices |
Will notify you when the hub lost connection to a Device. |
| Automations |
Will notify you when an automation has been triggered. |
| Devices |
Certain Devices can send notifications on their own. You can select the devices that are allowed to send notifications. TIP: You can also enable or disable notifications of a device in the device
options.
|
| PERSONAL | |
| Overconsumption |
The app will trigger an alarm when the device's usage exceeds the set limit, helping you to manage and reduce overconsumption effectively. Refer to Setting-up Overconsumption Alarm for information on how to set the overconsumption alarm. |
| No Consumption |
The app will trigger an alarm when the device consumes 0 watts for a set period of time. Refer to Setting-up No Consumption Alarm for information on how to set the no consumption alarm. |