Reduce my Bill - Expert rule
This feature automatically schedule the loads when the cost is
the cheapest. Shifting loads at low tariff periods reduces the energy
bill. Based on the tariff input, enabling this feature will automatically
switch the high-consuming devices ON during the cheapest electricity
rates and OFF during peak hours.
Pre-requisite
-
Commission one of your PowerTag as Grid. Refer to Pairing the main device.
-
Commission the supported devices. Refer to Pairing the Schneider Charge.
-
Set your peak/off peak tariff according as per your electricity contract. Refer to Setting tariff.
Once device is commissioned and the tariff is set, user gets notified in the Insights tab that this feature is available and also a push-notification is sent.
Enabling Reduce my Bill
To enable Reduce my Bill:
-
On the Home page, tap then tap banner (A).
IMPORTANT:-
Do not accidentally close the banner as it takes 2 weeks for this option to reappear.
-
If you close the banner again, a final reminder will appear after 6 weeks.
-
-
Read the tutorial information and tap Next twice, then tap Go to Reduce my Bill settings.
-
Enable the toggle switch for the devices you want to have this feature.
IMPORTANT:-
If you have closed the reminder banner, you can also enable the Reduce My Bill feature in the Settings page.
-
On the Home page, tap and follow step 3.
NOTE: After enrolling devices to RMB-AI, refer to Using Reduce My Bill to view how the devices are controlled and scheduled for usage. -
Disabling Reduce my Bill
To disable Reduce my Bill: