DUG_Schneider Charge_WHP-01

Network settings

If Wi-Fi network setting as changed, you can update the setting in Schneider Charge via Wiser Home app.
  1. On the Home page, tap All > Schneider Charge > Device settings.
  2. Tap Network Settings > Schneider Charge Network Setup > to update the network settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?