DUG_Schneider Charge_WHP-01

Pairing the device to Wiser Home app

IMPORTANT: Make sure that the Schneider Charge has been configured by a professional installer and pairing between Anti-Tripping Module and Schneider Charge is successful.
  1. On the Home page, tap .
  2. Tap Devices > > Energy.
  3. Select Schneider Charge and then tap Next on setup page.
  4. Select one of the following options to enrol your Schneider Charge using the charger ID.
    Open camera:
    Tap Open camera, on the pop-up message tap OK and scan the QR code located on the bottom left hand side of your Schneider Charge.
    IMPORTANT: Make sure the camera permission is enabled for Wiser Home app.
    Enter charger ID:
    Tap Enter charger ID to enter the 32 character charger ID located next to QR code on the bottom left hand side of your Schneider Charge and tap Enrol my charger.
    Wait for 5 min for the charger to get connected.
  5. Once connected, tap Name to enter the name based on your preference and then tap Next.
    NOTE: By default, the name will appear as Schneider Charge.
  6. Turn on the toggle switch to enable charging authorisation and then tap Next.
    If enabled, you can initiate the charging process by tapping Authorize charge in the control panel of the Wiser Home app after connecting the charger to an EV. If not enabled, the charging will start immediately upon connecting the charger to an EV.
    Refer Enabling charging authorisation for more info.
  7. Tap Finish to complete pairing process.
On successful pairing, the Schneider Charge will appear on the app's home page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?