Reduce My Bill - AI
Reduce my bill with Artificial Intelligence (hereinafter referred as RMB - AI) is a feature that allows users to save electricity costs by enrolling high energy devices like Schneider Charge. It is used with variable tariffs, such as peak/off-peak tariff, and relies on users to answer routine questions. The Al creates smart schedules for enrolled devices and limits the usage of these devices when electricity prices are high, while following user’s habits. It adapts the last 30 days of consumption data from the Grid.
-
Savings on electricity bills upto 10 %
-
Savings will be monitored on a daily, monthly and yearly basis.
-
The AI system learns by itself and benefits from historical data on electricity consumption. It can already optimize to some extent without pre-existing data, and its performance will improve significantly over time.
-
While this feature is active, RMB - AI schedules replace any customized schedules.
-
You can enroll one Schneider Charge.
Pre-requisite
-
Commission one of your PowerTag as Grid. Refer to Pairing the main device.
-
If you have installed solar panels in your home. Refer to Pairing the device with Energy storage system.
-
Commission the supported devices. Refer to Pairing the Schneider Charge.
-
Set peak/off peak tariff according as per the electricity contract. Refer to Setting tariff.