SUG_Wiser_Australia_WSE-07

Ethernet mode connection- Wiser Hub

  1. Locate the Ethernet port (A) on the hub.
  2. Connect an Ethernet cable between the hub and the router to suit the installation method used for the hub:
    • Wall mount using two screws (B)

    • Table mount using optional tablestand (C)

You must add the hub to the app before you can add devices to control them. To do this, first download and install the app on your mobile phone (see Downloading the app) and register a user account. You can then add the hub and optionally connect the hub to the network router by Wi-Fi.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.