SUG_Wiser_Australia_WSE-07

Connected switches

Wiser Micro Module Switch

Enables convenient multi-way switching by connecting up to 10 compatible momentary push-button switches.

NOTE: Momentary push buttons must be certified for use in 220-240 V AC applications. Voltage free contacts allow control of garage door or gate motors as well as lighting, exhaust fans and other loads. Use for non Iconic plates such as Saturn Zen. Also, ensure to lock all the doors to avoid accidental access.

Instruction Sheet (PDF)

Device User Guide

Iconic Connected Switch 10AX — Zigbee default mode

Controls the lights, fan motors or other loads from the push button in a room, or automatically switches the load On or Off in response to a specified condition or event.

Use with Iconic, Iconic Styl, Iconic Essence or Pro Series plates.

Instruction Sheet (PDF)

Device User Guide

Iconic Connected Switch 2AX –– Zigbee default mode

Controls the lights, fan motors or other loads from the push button in a room, or automatically switches the load On or Off in response to a specified condition or event.

Use with Iconic, Iconic Styl, Iconic Essence or Pro Series plates.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.