SUG_Wiser_Australia_WSE-07

Iconic Connected AC Fan Speed Controller, Zigbee/BLE

Symptom

Solution

No fan movement or uncontrolled movement.

  • Check power supply.

  • Check the wiring.

  • Check the load

The device is not ready to pair after the device is removed from the app.

Reset to factory default settings, refer to resetting the device manually.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.