SUG_Wiser_Australia_WSE-07

Switching the hub Ethernet connection to Wi-Fi (optional)

Use Wi-Fi to connect the hub to the network router so that the Ethernet cable is no longer needed.

Before doing this task, confirm that the mobile phone and hub are both connected to the Wi-Fi network router.

  1. In the app, select the hub to the same Wi-Fi network.
    NOTE: At this stage, the Ethernet cable should be still connected.
  2. Tap the Settings (gear) icon (A).

  3. In the Settings page, tap IP Network Setting(B).

  4. Tap the Wi-Fi tab, set the SSID and Password for the Wi-Fi network router and then tap Apply(C).

  5. Once the Wi-Fi connection is successful, remove the Ethernet cable from the hub .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.