SUG_Wiser_Australia_WSE-07

Device button/key and LED locations

Find the location of buttons, keys and LED indicators on various devices.

Wiser Micro Module Blind

The external push button is also the reset button. See the device instructions for more information.

NOTE: There is no LED indication.

   

Wiser Micro Module Dimmer

The external push button is also the reset button. See the device instructions for more information.

NOTE: There is no LED indication.

Wiser IR Convertor

(See A) Set/Reset (S/R) button

(See B) Network status LED

Wiser Window/Door Sensor

(See A) Function key

(See B) Status LED (visible on front of master part when flashing or lit)

Wiser Motion Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser Water Leakage Sensor

(See A) Function key

(See B) Status LED (visible on top of sensor when flashing or lit)

Wiser Temperature/Humidity Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser IP Camera Indoor

(See A) Micro SD Card slot

(See B) Status LED

(See C) Reset Button

Connected Switch 2AX

(See A) Operation button

(See B) Status LED

Connected Switch 10AX

(See A) Operation button

(See B) Status LED

Connected Dimmer

(See A) Operation button

(See B) Status LED

Connected Socket Twin 10A

The touch switch is also the reset button. See the device instructions for more information. The touch switch also has a left and right socket LED indicator, when is illuminated for 5 seconds each time a socket is turned on.

/ Wiser Smoke Alarm Lithium Battery Square/Wiser Smoke Alarm 240V Square

Smoke Alarm 240 V, works with Wiser

(See A) Reset button

(See B) Status LED

(See C) Standby LED

(See A) Reset button

(See B) Standby LED

(See C) Status LED

Iconic Connected AC Fan Speed Controller, Zigbee/BLE

See (A) Push-button/Reset button

See (B) Speed indicating LEDs

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.