SUG_Wiser_Australia_WSE-07

Room Control with Iconic BLE devices

Use the Wiser by SE App to set timers, schedulers or specific device features by pairing your smartphone to an Iconic connected device in BLE mode. When in the room, the end user can switch loads and dim lights through the Wiser by SE App or directly via the wall-mount switch. The Wiser Hub is not required.

For more information, refer to the installation instructions for the Iconic BLE default devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.