SUG_Wiser_Australia_WSE-07

Safety device

Wiser Smoke Alarm Lithium Battery Square

Smart Smoke Alarm 240 V

Smoke Alarm 240 V, works with Wiser

The Wiser Smoke Alarm - Battery uses a photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat by rapid increase in temperature. When connected to the Wiser system, the device will send the notifications via the Wiser app.

Instruction Sheet (PDF)

Device User Guide

The Smoke Alarm 240V, works with Wiser uses a photoelectric sensor to detect smoke generated by fire. It also includes a backup battery that allows the device to work if the power supply is disconnected. When connected to the Wiser system, the device sends notifications to the user via the Wiser app.

Instruction Sheet (PDF) — Square

Device User Guide — Square

Instruction Sheet (PDF) — Round

Device User Guide — Round

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.