990-6537E-001

Transfer the UPS from Static Bypass Operation to Normal Operation

  1. From the main menu, tap Control > Operation mode > Transfer to normal operation.
  2. Tap OK on the confirmation screen.
  3. If bypass is out of tolerance, a pop-up warning will show on the display.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.