990-6537E-001

View the Battery Solution Configuration

DANGER
hazard of electrical shock, explosion, or arc flash
Battery settings must only be entered by qualified personnel knowledgeable of batteries, battery configuration, and the required precautions.
Failure to follow these instructions will result in death or serious injury.
  1. From the main menu, tap Configuration > Battery.
  2. Tap General settings to view the following battery settings:
    Presence of battery breakers Shows the presence of the battery disconnect devices (BB1, BB2, BB3, and BB4). If the value is ‘Yes’, it means the battery disconnect device is present in the UPS system. Only configurable by Schneider Electric service.
    Low runtime warning (sec) Sets the threshold for remaining runtime in seconds that will activate the low runtime warning.
    Charge capacity (%) Sets the maximum charge capacity in percentage of the UPS nominal power rating.
    Temperature monitoring Shows if temperature monitoring is enabled. Only configurable by Schneider Electric service.
    Temperature sensor # 1/Temperature sensor # 2/Temperature sensor # 3/Temperature sensor # 4* Shows presence of temperature sensors. Only configurable by Schneider Electric service.
    Minimum threshold (°C)/
    Minimum threshold (°F)*
    Sets the minimum acceptable battery temperature in Celsius or Fahrenheit. Temperatures below this threshold will activate an alarm.
    Maximum threshold (°C)/
    Maximum threshold (°F)*
    Sets the maximum acceptable battery temperature in Celsius or Fahrenheit. Temperatures above this threshold will activate an alarm.
    Test interval every

    Sets how often the UPS should run an automatic battery test.

    Test day of the week

    Sets on which day of the week the automatic battery test should run.

    Test start time (hh:mm)

    Sets which time of day the automatic battery test should run.

    Manual battery self-test mode

    Selects the manual battery self-test mode.

    Time limit (minutes)

    Sets the maximum time for the manual battery self-test in voltage/time mode.

    Voltage limit setting in self-test mode

    Sets the minimum voltage for the manual battery self-test in voltage/time mode.

    • Lead-acid battery range: 1.7 – 2.3 V

    • Lithium-ion battery range: 3.5 – 4.1 V

  3. Tap Specific settings to view the following settings.
    NOTE: These settings are only configurable by Schneider Electric Service.
    Battery midpoint connected Shows if battery midpoint is connected.
    Disable temperature monitoring Shows if temperature monitoring is disabled.
    Allow boost charge Shows if boost charge is allowed. Boost charging makes it possible to conduct a fast charging in order to quickly restore a discharged battery.
    Allow battery deep discharge Shows if battery deep discharge is allowed. The deep discharge function allows to discharge the batteries to an even lower voltage level than the normally recommended value when in battery operation. Note that this may damage the batteries.
    Enable battery automatic disconnect Shows if battery automatic disconnect is enabled. When the UPS output is off and no ability to charge the batteries is available, this function will trip the battery disconnect devices to avoid battery deep discharge after a period of:
    • Two weeks, or

    • 10 minutes with the battery cell voltage below the low battery shutdown level.

    Battery capacity per battery block (Ah) Shows the battery capacity per battery block in ampere hours for the battery bank connected to each battery disconnect device.
    Number of parallel battery strings Shows the number of battery strings connected in parallel for the battery bank connected to each battery disconnect device.
    Number of battery blocks per string Shows the number of battery blocks per battery string.
    Number of battery cells per block Shows the number of battery cells per battery block.
    DC voltage per battery cell (V) Shows the float voltage.
    Float charging is the basic charging function available on all types of batteries and automatically initiated by the charger.
    Shows the boost voltage.

    Boost charging makes it possible to conduct a fast charging in order to quickly restore a discharged battery.

    Charge duration (sec) Shows the duration in seconds of the charge for Float charging and Boost charging.
    DC shutdown voltage per battery cell (V) Shows the voltage level per battery cell for when the battery must be shut down.
    Nominal temperature (°C) /
    Nominal temperature (°F)
    *
    Shows the nominal temperature.
    Charge current rate Shows the charge current rate.
    NOTE: Lithium-ion batteries do not support boost charge. The configurations for boost charging are not valid for Lithium-ion batteries.
    NOTE: Custom Lithium-ion batteries are not supported.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.