990-6537E-001

Tests

The UPS system can perform the following tests to ensure correct performance of the system:

  • Buzzer

  • Runtime calibration

  • Battery

From the main menu, tap Maintenance to access the tests of these functions. See Start a Runtime Calibration Test and Start a Battery Test for details and requirements for these tests.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.