990-6537E-001

Start Up the Single UPS with One Internal Switch from Maintenance Bypass Operation

NOTE: The following are generic start-up procedures. You can also follow the steps of the Guided sequences which are specific to your system. Select Control > Guided sequences > Start up UPS system and follow the steps which appear on the display.
  1. Generic start-up procedure for the single UPS using external maintenance bypass disconnect device Ext. MBB:
    1. Close UIB (if open).
      The display turns on. The rebooting sequence lasts approximately 3 minutes.
    2. Close SSIB (if present).
    3. Close the battery disconnect device(s).
    4. Select Control > Operation mode > Transfer to bypass operation if possible.
    5. Close UOB (if present).
    6. Confirm the self-test for the static bypass switch has completed.
    7. Open Ext. MBB.
  2. Generic start-up procedure for the single UPS system using internal maintenance disconnect device IMB (no Ext. MBB present):
    1. Close UIB (if open).
      The display turns on. The rebooting sequence lasts approximately 3 minutes.
    2. Close the battery disconnect device(s).
    3. Select Control > Operation mode > Transfer to bypass operation if possible.
    4. Confirm the self-test for the static bypass switch has completed.
    5. Open IMB.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.