990-6537E-001

Check the Status for the Power Module(s)

  1. From the main menu, tap Status > Power modules.
    1. If the power module is installed in the UPS and it is operable, a check mark will appear on the right of the corresponding icon on the screen.
    2. Tap the power module icon to view the detailed settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.