990-6537E-001

Configure the Modbus

  1. From the main menu, tap Configuration > Modbus > Serial Modbus.
    1. Enable or disable Serial Modbus.
    2. Set the Parity to None, Even, or Odd.
    3. Set the Stop bit to 1 or 2.
    4. Set the Baud rate to 2400, 9600, 19200, or 38400.
    5. Set the Target unique ID to a number between 1 and 247.
      NOTE: Every device on the bus must have exactly the same settings except the device address Target unique ID, which must be unique for every device. No two devices on the bus can have the same address.
    6. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.