990-6537E-001

Configure the Display Preferences

  1. From the main menu, tap Configuration > General.
    1. Set the Start screen saver time after (minutes). After the set minutes of no activity, the screen saver will begin on the display.
    2. Set the temperature unit to Celsius or Fahrenheit.
    3. Tap the - or + to set the display brightness.
    4. Set the Alarm sound to Enable or Disable. This will enable/mute all alarm sounds.
    5. Set the Touch screen sound to Enable or Disable. This will enable/mute all display sounds (excluding alarm sounds).
    6. Tap the Calibration button twice to calibrate the display.
  2. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.