990-6537E-001

Shut Down the Parallel UPS System into Maintenance Bypass Operation – for UPSs with One Internal Switch

NOTE: The following is a generic shutdown procedure. All the disconnect devices mentioned may not be present in your specific system.
  1. Make sure IMB is open.
  2. Select Control > Operation mode > Transfer to bypass operation if possible.
  3. Close Ext. MBB.
  4. Open SIB (if present).
  5. Open UOB (if present).
  6. Open SSIB (if present).
  7. Open the battery disconnect device(s).
  8. Open UIB.
  9. Repeat step 5 to 8 for the other UPSs in the parallel system.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.