990-6537E-001

Overview of User Interface

Display

Overview of the Home Screen

  1. Home button - tap here on any screen to return to the home screen.

  2. Main menu button - tap here to access the menus.

  3. Mimic diagram button - tap here to access the mimic diagram.

  4. Alarm status symbol - tap here to access the active alarms log.

You can tap on the output or battery fields on the home screen to go directly to the detailed measurement pages.

Main Menu


Tap the main menu button on the home screen to access the menus.

Mimic Diagram

Tap the mimic diagram button on the home screen to access the mimic diagram.

The mimic diagram will adapt to your system configuration – the mimic diagram shown here is just an example.

Example of Single UPS System (UPS with One Internal Switch) – Single Mains

Example of Single UPS System (UPS with Four Internal Switches) – Single Mains

The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.

NOTE: The mimic diagram only shows one battery disconnect device BB even if more battery disconnect devices have been connected and configured for monitoring. If one or more of the monitored battery disconnect devices are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery disconnect devices are in the open position, the BB on the mimic diagram will show as open.

In mimic diagrams for parallel systems, tap on the gray UPS to see the mimic diagram on UPS level.

Example of Parallel System – Single Mains with Individual UIB

Example of Parallel System – Dual Mains with Individual UIB and SSIB

Alarm Status Symbols

The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.

Green: No alarms present in the UPS system.
Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Connection from the display to the UPS is lost.

Menu Tree


Tap the main menu button on the home screen to access the menus.

  • Status

    • Input

    • Output

    • Bypass

    • Battery

    • Temperature

    • Power modules

    • Parallel

    • Redundant IM

  • Logs

  • Control*

    • Operation mode

    • Inverter

    • Charger

    • Guided sequence

  • Configuration*

    • UPS

    • Output

    • Battery

    • High efficiency

    • Contacts and relays

    • Network

    • Modbus

    • General

    • Reminders

  • Maintenance

    • Buzzer

    • Battery*

    • Runtime calibration*

    • Battery replacement*

    • UPS report*

  • About

    • UPS

    • Display

    • Network management card (NMC) number 1

    • Network management card (NMC) number 2

  • Logout

  • Digital experience

  • Language

Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.

Controller Section

Overview of Signal Connection Terminals in the UPS

  1. Remote EPO (J6600)

  2. Display port (for internal use)

  3. USB port (for service)

  4. Tuner port (for service)

  5. Modbus port

  6. Battery temperature sensor (J3008)

  7. Input contacts (J3009)

  8. Output relays (J3001)

  9. PBUS2

  10. PBUS1

  11. Network management card (NMC) slot 1

  12. Network management card (NMC) slot 2

  13. IM1 slot for intelligence module

  14. IM2 slot for intelligence module

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.