990-6537E-001

Stop a Battery Test

  1. Tap the menu button on the home screen.
  2. Select Maintenance > Battery > Stop test.
  3. Tap OK on the confirmation screen. If the test process stalls, click the Abort button to exit the battery test.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.