990-6537E-001

Start a Battery Test

Prerequisites:

  • No battery test is running.

  • The battery disconnect devices are closed.

  • No critical alarms present.

  • The bypass supply must be available.

  • Static bypass operation must be available.

  • The batteries must be more than 50% charged.

  • The runtime available must be more than 4 minutes.

  • The operation mode must be normal operation.

  • The system operation mode must be inverter.

This feature performs a number of tests on the batteries, such as fuse-blown check and weak battery detection. The test will discharge the batteries and use about 10% of the total runtime capacity. Example: If you have 10 minutes of runtime, the test will run for 1 minute. The battery test can be scheduled to run automatically in different time intervals (from weekly and up to once a year).

  1. From the main menu, tap Configuration > Battery > Manual battery self-test mode and select the manual battery self-test mode: By capacity (automatic or manual battery tests) or By voltage/time (only for manual battery tests).
  2. Tap Maintenance > Battery > Start test.
  3. Tap OK on the confirmation screen.
  4. When the battery self-test starts, the message ‘Battery self-test is running’ will show on the display and will remain on the display until the completion of the battery self-test. Click the Abort button to abort the automatic battery self-test.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.