990-6537E-001

Replace the Display

NOTE: The display can be replaced when the UPS is in any operation mode.
  1. Open the front door.
  2. Disconnect the cables from the display.
  3. Remove the fixing bracket of the display by removing the six clips in the indicated locations. Loosen the clip fixing screws completely with a Phillips screwdriver and remove the clips.
  4. Install the replacement display and fasten with the fixing bracket and six clips. Reconnect the cables.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.