990-6537E-001

Configure the Network

  1. From the main menu, tap Configuration > Network.
  2. Select Network management card (NMC) number 1 > IPv4 to configure network management card number 1 or Network management card (NMC) number 2 > IPv4 to configure network management card number 2.
    1. Set the Address mode to Manual, BOOTP, or DHCP.
    2. You can also disable the network by selecting Disable IPv4 for NMC no. 1/Disable IPv4 for NMC no. 2.
    3. Tap OK to save your settings.
    4. Tap Network to return to the previous screen. Tap Reboot NMC1 or Reboot NMC2 to reboot the network management card to implement the changes.
  3. Tap Configuration > Network. Select Network management card (NMC) number 1 > IPv6 to configure network management card number 1 or Network management card (NMC) number 2 > IPv6 to configure network management card number 2.
    1. Set the DHCPV6 mode to Address and other information, Non-address information only, or IPv6 never.
    2. Select Auto configuration or Manual.
    3. You can also disable the network by selecting Disable IPv6 for NMC no. 1/Disable IPv6 for NMC no. 2 .
    4. Tap OK to save your settings.
    5. Tap Network to return to the previous screen. Tap Reboot NMC1 or Reboot NMC2 to reboot the network management card to implement the changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.