990-6537E-001

System Modes

The system mode indicates the output status of the complete UPS system including the surrounding switchgear and indicates which source supplies the load.

Inverter Operation

In inverter operation the load is supplied by the inverters. The UPS mode can be in either normal operation or battery operation when the system operation mode is inverter operation.

Requested Static Bypass Operation

When the system is in requested static bypass operation, the load is supplied from the bypass source. If a fault is detected, the system will transfer to inverter operation or forced static bypass operation.

Forced Static Bypass Operation

The system is in forced static bypass operation following a command from the UPS system or because the user has pressed the inverter OFF button on the UPSs. During forced static bypass operation, the load is supplied directly by the bypass source with unconditioned power.

NOTE: The batteries are not available as an alternate power source while the system is in forced static bypass operation.

Maintenance Bypass Operation

In maintenance bypass operation, the load is supplied directly by the bypass source with unconditioned power.

NOTE: The batteries are not available as an alternate power source in maintenance bypass operation.

ECO Mode

ECO mode allows the system to be configured to use requested static bypass operation, with the load supplied through the bypass, as the preferred operation mode under predefined circumstances. The main advantage of ECO mode is a reduction in the consumption of electrical power. In case of interruption to the utility/mains supply, the UPS transfers to inverter operation for an uninterrupted supply of the load.

NOTE: ECO mode is not supported in parallel system.

OFF Mode

The system is not supplying the load with power. The batteries are charged and the display is on.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.