990-6537E-001

Configure the UPS Output

NOTE: This configuration is mandatory for correct UPS operation.
  1. From the main menu, tap Configuration > Output.
    1. Set the AC voltage ph-ph to 380 VAC, 400 VAC, or 415 VAC depending on your configuration.
    2. Set the Frequency to 50 Hz ±1.0, 50 Hz ±3.0, 50 Hz ±10.0, 60 Hz ±1.0, 60 Hz ±3.0, or 60 Hz ±10.0 depending on your configuration.
    3. Tap OK to save your settings and tap the arrow symbol to go to the next page.
    4. Set the Output RMS voltage tolerance (%). The output RMS voltage tolerance range is +3% to +10%, default is +10%.
    5. Set the Overload threshold (%). The overload warning range is 0% to 100%, default is 75%.
    6. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.