990-6537E-001

Isolate a Single UPS with One Internal Switch from the Parallel System

Use this procedure to shut down one UPS in a running parallel system.

NOTE: Before initiating this procedure, ensure that the remaining UPSs can supply the load.
NOTE: The following is a generic shutdown procedure. All the disconnect devices mentioned may not be present in your specific system.
  1. On this UPS, select Control > Inverter > Inverter off. Tap OK on the confirmation screen.
  2. Open UOB for this UPS.
  3. Open SSIB (if present) for this UPS.
  4. Open the battery disconnect device(s) for this UPS.
  5. Open UIB for this UPS.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.