990-6537E-001

Configure the Air Filter Reminder

When the air filter has been replaced, reset the air filter reminder.
  1. From the main menu, tap Configuration > Reminders.
    1. Select Enable reminder to get reminders about replacing the air filter.
    2. Select the reminder interval: 1 month, 3 months, 6 months, or 1 year based on the installation room environment.
      Under Remaining time (weeks) you can see how much service life the air filter in use has left.
    3. Tap Reset to reset the air filter service life counter.
  2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?