990-6537E-001

Disconnect Device Explanation

IMB Internal maintenance disconnect device
UIB Unit input disconnect device
SSIB Static switch input disconnect device
UOB Unit output disconnect device
SIB System isolation disconnect device
BIB Bypass input disconnect device
MIB Main input disconnect device
BB Battery disconnect device
MBB Maintenance bypass disconnect device
Ext. MBB External maintenance bypass disconnect device
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.