990-6537E-001

Export UPS Event Logs to a USB Device

  1. From the main menu, select Maintenance > UPS report.
  2. Open the front door.
  3. Insert your USB device in the USB port on the display.
  4. Tap Export. When the screen shows the message Confirm to export UPS event logs, tap OK to start the export process.
    NOTE: Do not remove the USB device until the export process has finished.
  5. The screen will show the completion status with the message Event dump successful or Event dump unsuccessful. Tap OK to proceed.
  6. Send the UPS event logs to Schneider Electric customer support.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.