990-6537E-001

Live Swap: Add, Remove, or Replace a Power Module, Static Bypass Switch Module, and Display

NOTE: This UPS has been designed and evaluated for:
  • Power module insertion and removal in any operation mode: Live Swap.

  • Static bypass switch module insertion and removal in normal operation or battery mode: Live Swap.

  • Display insertion and removal in any operation mode: Live Swap.

This section specifies manufacturer’s instructions for how to perform Live Swap.
NOTE: Verify that the required upstream protection is installed and configured correctly according to the installation manual.
NOTE: Incident energy is <1.2 cal/cm2 when installed and first startup commissioned in accordance with product instructions. Incident energy is evaluated 300 mm from cabinet front.

DISCLAIMER:

  • Electrical equipment should be installed, operated, serviced, maintained, replaced, or have similar work carried out on it only by suitably qualified, trained, experienced, and competent personnel who hold any necessary authorizations (e.g. licenses, permits or certifications) to perform such work. All work must be carried out in a way that does not give rise to danger and using appropriate personal protective equipment (PPE). 

  • User must ensure compliance with the manufacturer’s instructions and user manual and with all applicable laws, regulations, standards, and guidance when using this equipment and carrying out work or permitting work to be carried out on or near electrical equipment.

  • Neither Schneider Electric nor any of its affiliates shall be liable for any claims, costs, losses, damages, death, or injuries arising out of the improper use of this equipment or any failure to comply with any of the above requirements.

DANGER
Hazard of electric shock, explosion, or arc flash
  • Verify that the UPS has the Live Swap label present.
  • If no Live Swap label is present on the UPS, contact Schneider Electric for power module, static bypass switch module, and display replacement.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices.
  • Persons must not be present behind the UPS during this procedure.
  • Insertion or removal of power modules, static bypass switch modules, and display must only be performed by qualified personnel knowledgeable of electrical work and the required precautions. Keep unqualified personnel away.
  • This procedure requires opening the front door. All other doors and covers must remain closed and secured during this procedure.
  • Verify that the UPS is secured against movement before performing this procedure.
  • If evidence of poor maintenance or poor installation is observed, do not proceed with this procedure.
  • Do not install power modules, static bypass switch modules, and displays which have been accidentally dropped, broken, flooded, contaminated, infested, or damaged in any way.
  • Do not install power modules, static bypass switch modules, and displays which are of unknown operational state.
  • Keep a minimum distance of 300 mm from the cabinet front while the system is energized.
  • Do not use any tools inside the empty slots of power modules or static bypass switch modules.
  • Do not reach into the empty slots of power modules or static bypass switch modules.
Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.