990-6537E-001

Find the Serial Numbers

  1. From the main menu, tap About.
  2. Note down the serial number of the UPS cabinet and have it ready for customer support.
    NOTE: If the display is not available, open the front door to find the UPS serial number on the name plate label under SERIAL:

    Example of Name Plate Label for UPS

  3. Tap the arrow to go to the next pages and note down the serial numbers of the display and the network management card(s) and have them ready for customer support.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.