990-6537E-001

UPS Modes

Normal Operation

In normal operation, the UPS supports the load with conditioned power.

Battery Operation

If the utility/mains supply fails, battery power ensures uninterrupted support to the critical load during battery operation.

NOTE: When battery is supplying the UPS and no mains sources are available: If you disconnect the battery power, you must wait until all UPS power modules have completely shut down, before reconnecting the battery power to the UPS.

Requested Static Bypass Operation

The UPS can be transferred to requested static bypass operation following a command from the display. During requested static bypass operation, the load is supplied from the bypass source. If a fault is detected, the UPS will transfer to normal operation or forced static bypass operation. If there is an interruption to the utility/mains supply during requested static bypass operation, the UPS will transfer to battery operation.

Forced Static Bypass Operation

The UPS is in forced bypass operation when the UPS has detected an inoperable state on the system and requests static bypass operation or because the user has pressed the inverter OFF button on the UPS. During forced static bypass operation, the load is supplied from the bypass source.

NOTE: The batteries are not available as an alternate power source while the UPS is in forced static bypass operation.

Internal Maintenance Bypass Operation via the Internal Maintenance Disconnect Device IMB (for UPS with One Internal Switch)

When the internal maintenance disconnect device IMB is closed, the UPS transfers to internal maintenance bypass operation. The load is supplied with unconditioned power from the bypass source. Service and replacement can be performed on power modules and the static bypass switch module during internal maintenance bypass operation via the internal maintenance disconnect device IMB. The internal maintenance disconnect device IMB can only be used in single systems with no external maintenance bypass disconnect device.

NOTE: The batteries are not available as an alternate power source while the UPS is in internal maintenance bypass operation.

Internal Maintenance Bypass Operation via the Maintenance Bypass Disconnect Device MBB (for UPS with Four Internal Switches)

When the maintenance bypass disconnect device MBB is closed, the UPS transfers to internal maintenance bypass operation. The load is supplied with unconditioned power from the bypass source. Service and replacement can be performed on power modules and the static bypass switch module during internal maintenance bypass operation via the maintenance bypass disconnect device MBB. The maintenance bypass disconnect device MBB can only be used in single systems with no external maintenance bypass disconnect device.

NOTE: The batteries are not available as an alternate power source while the UPS is in internal maintenance bypass operation.

External Maintenance Bypass Operation via the External Maintenance Bypass Disconnect Device Ext. MBB

When the external maintenance bypass disconnect device Ext. MBB is closed in the external maintenance bypass panel/cabinet or third party switchgear, the UPS transfers to external maintenance bypass operation. The load is supplied with unconditioned power from the bypass source. Service and replacement can be performed on the entire UPS during external maintenance bypass operation via the external maintenance bypass disconnect device Ext. MBB. For more information, see Shut Down the Single UPS with One Internal Switch into Maintenance Bypass Operation and Shut Down the Parallel UPS System into Maintenance Bypass Operation – for UPSs with One Internal Switch.

NOTE: The batteries are not available as an alternate power source while the UPS is in external maintenance bypass operation.

Static Bypass Standby Operation

Static bypass standby is only applicable to an individual UPS in a parallel system. The UPS enters static bypass standby operation if the UPS is prevented from entering forced static bypass operation and the other UPSs of the parallel system can support the load. In static bypass standby the output of the specific UPS is OFF. The UPS automatically transfers to the preferred operation mode when possible.

NOTE: If the other UPSs cannot support the load, the parallel system transfers to forced static bypass operation. The UPS in static bypass standby operation will then transfer to forced static bypass operation.

Battery Test

The UPS is in battery test mode when the UPS is performing a battery self-test or a runtime calibration.

NOTE: The battery test will be aborted if the utility/mains supply is interrupted or if a critical alarm occurs and the UPS will return to normal operation upon return of utility/mains.

ECO Mode

ECO mode allows the UPS to be configured to use requested static bypass, with the load supplied through the bypass, as the preferred operation mode under predefined circumstances. If a fault is detected (bypass voltage out of tolerance, output voltage out of tolerance, etc), the UPS will immediately transfer to normal operation or forced static bypass. The main advantage of ECO mode is a reduction in the consumption of electrical power. In case of interruption to the utility/mains supply, the UPS transfers to battery operation for an uninterrupted supply of the load. The batteries are charged when the UPS is in ECO mode.

NOTE: ECO mode is not supported in parallel system.

OFF Mode

The UPS is not supplying the load with power. The batteries are charged and the display is on.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.