990-91077K-037

反向馈电箱重量和尺寸

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
SP3OPT008 20 300 550 200
SP3OPT009 33 600 600 250
SP3OPT010 58 800 700 400
反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.