990-91077K-037

反向馈电箱运输重量和尺寸

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
SP3OPT008 30 530 780 460
SP3OPT009 48 835 835 510
SP3OPT010 76 940 1050 660
注: 运输重量和尺寸是指在木制托盘上放置一台设备时的重量和尺寸。
反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.