990–5809D-001

Final Mechanical Assembly

Final Mechanical Assembly of the I/O Cabinet

  1. Install the plate in the top right corner of the I/O cabinet.

    Front View of the I/O Cabinet

  2. Close the door with the printed circuit boards and fasten with two screws.

    Front View of the I/O Cabinet

  3. In bottom entry systems only, install the plate at the bottom of the I/O cabinet.
  4. Install the plate at the top of the I/O cabinet.
  5. Install the nine indicated plates.

    Front View of the I/O Cabinet

  6. Close the front door.

Final Mechanical Assembly of the Power Cabinets

  1. Reinstall the three plates in the top of each of the power cabinets in chronological order (a-c).

    Front View of the Power Cabinet

  2. Reinstall the plate in each of the power cabinets.

    Front View of the Power Cabinet

  3. Push the two power blocks into each of the power cabinets and fasten with the screws.

    Front View of the Power Cabinet

  4. Reconnect the two cables to each of the two middle power blocks.
  5. Reinstall the fan doors and reconnect the cable between the fan doors and each of the power cabinets.

    Front View of the Power Cabinet

  6. Close the fan doors and fasten them to each of the power cabinets with the 12 screws.

    Front View of the Power Cabinet

  7. Close the front door.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.