990–5809D-001

Connect External Synchronization

The signal cables must have a minimum rating of 600 V.

  1. Open the door to ensure that the cables will not be too tight.
  2. Route the external synchronization cables through the top or bottom of the I/O cabinet to 0P6549 as shown in Prepare the I/O Cabinet for Signal Cables in Top Cable Entry Systems and Prepare the I/O Cabinet for Signal Cables in Bottom Cable Entry Systems.
  3. Connect the three phases:
    NOTE: The phases from the synchronization source must be protected by a fuse of maximum 0.5 A.
    1. Connect L1 to J5611 on 0P6549.
    2. Connect L2 to J5612 on 0P6549.
    3. Connect L3 to J5613 on 0P6549.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.